Hi team,
I want to confirm that the TPS25200 is not damaged under the following conditions.
Condition
FAULT# pin is forced 0V by another devices.
6pin IN : 0V or 3.3V or 5V
4pin EN : 0V or 3.3V
*Not required over current detection about these conditions.
My understanding is TPS25200 does not damaged, because FAULT# is open drain.
Regards,
Ogasawara