Other Parts Discussed in Thread: BQ40Z50
Hi,
I'm having issues with the SoH calculation when I am tweaking a cell-pack drastically. Meaning I have a cell-pack 4S6P with a max capacity of 20Ah (2.5V - 4.2V) but I only want to use about 11Ah, testing shows a voltage range from 3.2 - 3.9V gives me about 11600mAh of capacity (total delta QmaxPassedQ) but my SoH shows for example 72%.
I've set the DesignCapacity 10600mAh and first instance the Qmax (Cellx) also. Changing the Qmax to 19000mAh did not solve it. Qmax Delta is set to 100%, Qmax Upperbound is set to 190%. After this the Qmax (Cellx) has learned the actual capacities but the Full Charge Capacity remains low although when testing there is enough capacity compared to the
What settings must be made to get the correct SoH and Full Charge Capacity?
Thanks,
Rob Ploeg