This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR16020: Is it possible to reduce the integrated Soft Start in the SPICE model?

Part Number: LMR16020

Hi,

I'm currently simulating a SMPS design using LMR16020. I'm trying to do an AC Sweep in order to get a Bode Plot to evaluate the stability of the design.

However, simulations takes quite a while (~10min to simulate 10ms). I would assume the is due to PSpice also running all the UVLO and OVLO features of LMR16020.

I was wondering if it is possible to edit the SPICE model, to reduce the integrated soft start of 4ms, in order to reach steady-state faster and shorten simulation times?