This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS610981: lower cost solution

Part Number: TPS610981


Dear Team,

customer is checking for the lower cost solution to the TPS610981

with the following spec requirement, please help comment if there is more suitable solution.

Thanks

1. for CR2032 battery

2. output voltage  fixed at 3.3V (same as nrf528322)

3. efficiency above 90%

4. low consumption (<5uA at no load)