This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5088: LM5088

Part Number: LM5088


Hi TI,

we are using LM5088-1 to create +5.3VDC. Input voltage is 24V and it draws 0.2A with the load we have. The design is based on the component values from webbench. Our problem is that some of the powers will not start at -20C. In this case it draws 30mA. There are pulses on the gate of the MOSFET in this case.

Do you have any proposals how we should proceed to find the reason? The problem is that we cannot search for the reason on the labbench in an easy way.

Are there any component changes we should try out (connected to ramp, soft start, boot etc.) ? 

Capacitance on input is 3x100uF. On 5VDC side it is 2x330uF. Load is mainly resistive-capacitive

Regards Trond Inge WAng