Other Parts Discussed in Thread: TLV61046
I used TLV61046A to convert one cell Li-On battery to 5 V with maximum 0.3 A at output. And I need to disconnect battery to keep its charge longer after turn off.
In spec for TLV61046A mentioned: True Disconnection between Input and Output during Shutdown.
But when I put 0 V on EN input I have 0.85 V at output. The current from battery is about 200 uA not less then 10uA as expected. When EN=1 Output voltage is 5 V. The EN voltage goes from Flip-Flop.
Even I create EN=O V by peace of wire the same 0.85 V I have at DC-DC converter Output.