Other Parts Discussed in Thread: BQSTUDIO, EV2400,
Hello,
I was setting up the BQ25713EVM-017 evaluation board along with EV2400. I am using BQStudio v1.3.86 build date June 8,2018. When I click the read register button after changing the update mode to Manual, BQStudio raises a "Device ACK Error". I double checked the connections and the eval board is indeed connected to I2C port on the EV2400. I am using the file "Charger_1_00-bq25713_APL.bqz" as suggested in one of the previous forum posts but it still raises this error.
Any help resolving this issue will be appreciated.
Thanks,
Nosherwan