Hello,
this question is pretty urgent because we have several battery packs with the same behavior; all they are in PF status with DFETF set but testing the board, the MOSFET appears not damaged and there are no further way to drawn current in discharge if the DSG FET is open. The CHG & DSG FET is the CSD87313.
I would like to say that sometime we face the same problem during the test post-assembly of the cell to the board, but they are due the not correct handling of the boards after testing.
When the issue arrives from closed batteries that have already worked on field long times, 200 cycles or more, I do not know how to understand what has triggered the PF while the DSG FET is not damaged.
Another strange situation is that the packs shows RemainCapacity and FullCharge Capacity both 0 mA but the RSoC is 100%. I attach the .gg.csv file from one of those packs.
Thank you for explanation.
PS: what are the events that trig the SS bit? Are they the same or different from events which trig the PF bit?
/cfs-file/__key/communityserver-discussions-components-files/196/1s3p-_2D00_-PF-set.gg.zip