I’m trying to make the TPS65950 to Wait-ON state but the device is automatically restarting after writing into DEVOFF register.
The design is as below
PWRON – Pulled up to VBAT
VAC and VBUS both are supplied 5.0V through USB
AC Charger circuit present
When the VAC is not supplied and VBUS alone supplied, the device is not restarting till the pulse is given to PWRON.
After making the STARTON_CHG bit to 0 in CFG_P1_TRANSITION, CFG_P2_TRANSITION and CFG_P3_TRANSITION registers, the device is not restarting after writing into DEVOFF register when the VAC is present.
Does this mean if the VAC is present, the device will start automatically in the default configuration.