Hi TI,
I am working on a design with this part charging by PV Panels and AC to DC adapter. I’ve reviewed thread related to my issue and hope to get some advice.
PV panel is main input and AC to DC adapter is additional source of input if it’s possible to access to grid in the venue of installation sites. 4SNP LiFePO4 battery Pack (12.8V) is attached.
I wonder what is the proper voltage and ampere of AC to DC Adapter when voltage and ampere of PV panel is as follows.
-Vmp: 18.5V, Amp: ~8A(depends on Wattage of PV Panel), Voc: 21.9V
1. Is it suitable to use 24V, 8A AC to DC Adapter? 24V is more than Vmp of PV panel and less than 33V. If not, I hope to get your advice.
2. What about the Ampere of AC to DC Adapter I’m considering? Is the Ampere too high?
3. Is it necessary to use AC to DC Adapter providing CC and CV DC output?
Regards,
Jeong, Jake