This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: SHDN pin

Part Number: TPS1663

HI, 

For the SHDN pin, in the datasheet,  it is written "Pulling SHDN low makes the device to enter into low power shutdown mode. Cycling SHDN pin voltage resets the device that has latched off due to a fault condition".

I am not very clear about it. If I want to enable this chip, do I need to give a voltage like 4V to this pin? Or can I float this pin? I use this eFuse on the high voltage secondary side of my converter, so to find a 4V may become a problem, or can I just use a voltage divider to provide a 4V with no current capability?

For reset the latch off, what should I do? Is it correct to connect to the GND by a OFF-MOM switch?

Thank you for you patience and help.

Keyao