Other Parts Discussed in Thread: BQSTUDIO, GPCCHEM
Hello,
I have recently tried to implement a gauge on the Samsung INR-18650 -25R (CHEMID: 2068) in order to log state of charge and voltage while discharging at a constant 500 mA (C/5)
However, I have been able to successfully log only the Voltage of the cell. The state of charge drops from 100% to 0% while the battery is around 3.5V which should not be the case at it should go down to 0% at around 2.8V. Also in my log file, the discharge current stays at -500 mA which is the calibrated value and not the actual measured value.
I have seen something about a learning cycle but I dont see an option to configure one. Also, I am not certain about the level of detail the calibration requires in order to gauge properly.
I am very new to the EVM2400 any help would be appreciated.
Thank you!
regards,
Yannis