This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ33100: Can device be used with two supercapacitors in parallel?

Part Number: BQ33100
Other Parts Discussed in Thread: BQ24640,

Hi,

Can device be used with two supercapacitors in parallel? I have two Maxwell BCAP 1200F supercapacitors which I would like to place in parallel. They will be charged using the BQ24640. Would I be able to use the BQ33100 to monitors the caps and control the charging? Would I lose some features or would the monitoring not work at all?

Thank you