This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC59116: About LED current accuracy with series LEDs

Guru 11170 points
Part Number: TLC59116


Hello E2E,

Our customer is using this device in experimental board.
They added from single LED to two series LEDs per /OUT channel.
So, LED current error is to be large more than single LED.

Current error
  -  Single LED : less than 8%
  -  Two series LEDs : 8.2%

Please tell me the reason why the LED current error increases by series LEDs number.

Possibly, is this device for no series LEDs?

Regards,
ACGUY