Hi Sir,
Here is a question about the current detect accuracy.
Background: BQ27510-G3, current sense resistor = 0.01 ohm.
Can gauge detect the current that passes through the sense resistor like 0.2mA?
I think this current detect accuracy is related to ADC (coulomb counter) characteristics, so I find the INL of this ADC from the datasheet as below. then I calculated the detect current accuracy, the typical is 0.175mA, the max is 0.85mA. Is this method right form your opinion? Do you have some information of the minimum current that this gauge can detect?
And the deadband also affect the current detect accuracy, so if the deadband is 68, how about the minimum current that this gauge can detect?
Thank you.
Penn