Hello guys,
Could you help me to explain more about the BQ24707 IC?
Now I was successfully configured the IC over SMBus communication and all scenarios happen to seem to be right with the datasheet. However, I was wondering about the max power that the BQ24707 can adapt to charge for the battery.
In my testing, the input power is adapter 20V-3A, the output is two lithium battery which has capacity 5000mAh so I config charge voltage level is 8.4V and set the charge current goes to maximum value.
I expect that BQ24707 can charge the two battery in 5A current level but when I measured the reality result which is less than 4A. According to the document, the BQ24707 can output charge current higher than 8A if we use output capacitor > 30 ( we had already done that).
So anyone can answer to me that what is maximum charge current output of BQ24707 with 2-cell battery?
Thank you.
Regards
----------------------------------------------------------------------------------------
Personal contact: 0942781347
Company: HomeIQ Việt Nam