This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CISPR 22/24 Class B of Buck DCDC

Other Parts Discussed in Thread: TPS54360B, LMR16030, PMP15013

Please tell us the recommended device that meet the following conditions.

Vin=30~60V

Vout=5V

Iout=4A

Compliant CISPR 22/24 Class B

Either isolated IC or non-isolated IC may be used.

Does TPS54360B compliant CISPR 22/24 Class B?

Best regards,

Takahiro Nishizawa