For the Setup: I change R13 to 100kOhm, so that I have an output voltage of 4.2V.
I follow the measurement protocol as described in 2.7.1.
-as expected I measured V_sys=21V, V_ref= 3.3V, V_regn=0V, but V_Out=1.6V and not 0V.
-When I switch off the voltage source, a capacitive discharge curve is shown.
In the next step followed the measurement protocol as described in 2.7.2.
-All the voltages behaved as expected. V_REF=3.3V,V_regn=6V,V_out=4.1V (I changed R13), but D4 (State1) turned on.
Based on this Behavior and on the fact, that the IC didn't charge the Battery. I measure all components and found a short connection between the Gate and the Source of Q1.A.
I hope you can help me. I didn't changes no other components expect R13.