Other Parts Discussed in Thread: BQ24650
A PCB with the BQ77915 protection and BQ24650 charger is not recovering by load removal.
When I plug in the charger, which is directly attached to the pack via protection on the PCB, the pack recovers.
I would like to get the load removal recovery working as well.
From what I understand from the datasheet, once OCD is triggered, LD pin wants to pull low.
If there is a load attached which pulls up, that is not possible. Apparantly the charger is seen as a load.
I measured the LD pin voltage on the PCB after OCD was triggered, which was 3.6V (Rld=500k)
I increased Rld to 3.3M, so that Vld can go below 1.25V to trigger recovery, but now OCD does not trigger at all.
What would be a good solution?