This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MC34063A: The input of VBUS is 5V, 2.4A,the output is 12V,1A

Part Number: MC34063A
Other Parts Discussed in Thread: TPS61087, TPS61089

Dears:

Could you kindly help to check the schematic as follows:

The input of VBUS is 5V, 2.4A,the output is 12V,1A.