This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50EVM-561: Detecting wrong number of cells

Part Number: BQ40Z50EVM-561
Other Parts Discussed in Thread: BQ40Z50, BQSTUDIO

Hello,

I just started working with the EVM for BQ40Z50. I set up everything according to the user guide and am using 3 resistors to simulate a 3S configuration for Li-ion battery.  The pack+ and pack- are coming from the power supply @ 10.8V (3.6V per Li-ion cell). However when i open up bqStudio, it shows 0V for cell 3 and cell 4 which leads me to believe that it thinks only two cells in series are connected but that is not the case. I double checked the CC bits in the DA Configuration register and it is indeed set to (10)b .Can anyone help to figure out a solution to this issue?

Thanks

Nosherwan