Hi Every one ,
As im planning to use DC source (120VDC) to power up the smps. As far as my understanding there is not big difference in using DC apart from considering fuse and EMI filter .
Please advise
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Every one ,
As im planning to use DC source (120VDC) to power up the smps. As far as my understanding there is not big difference in using DC apart from considering fuse and EMI filter .
Please advise
Hello Balasubramani R,
This is a very good question.
The standard U.S. AC outlet voltage is 120VAC rms +-10%
The peak voltage is Vrms x sqrt 2 = Vrms x 1.414.
120Vrms = 170Vpeak
240Vrms = 340Vpeak
Many devices that use AC wall power have a simple bridge rectifier or bridge doubler at the input.
The bridge rectifier will peak detect the AC, creating a voltage that is 170DC with a lower valley due to ripple.
DC voltage will pass through the bridge.
Thus you need an ~170VDC source to equal the rectified 120VAC voltage.
However if the SMPS has a bridge doubler on the input there will be problems.
As the picture below shows, when the switch is in 117V (U.S.) it acts as a voltage doubler however it only doubles on AC input, not DC.
TI Power Supply Design Seminar Resources
http://www.ti.com/ww/en/power-training/login.shtml?DCMP=pwr-psds-archive&HQS=pwr-psds-archive-psds
Line Input AC to DC Conversion and Input Filter Capacitor Selection
http://www.ti.com/lit/slup060
When in the doubler mode, switch closed, applying a positive DC voltage will only charge C1 of the 2 series input capacitors.
Circuits like this are common in consumer electronics.
Desktop PC’s is a good example, most have a 110/220 switch on the rear of the system.
The SMPS therefore is expecting a Vbus of 340VDC.
You can place the switch in 230V mode and apply a 340VDC and the SMPS might work.
However if the SMPS employs a PFC Power Factor Correction circuit on the input, then applying a DC input will likely not work. The PFC circuit is expecting AC, not DC.
Another issue can be that some SMPS may have other housekeeping circuits that rely on an AC input.
Yes the EMI filter does not really care if it sees AC or DC.
The rest of the SMPS might.
Bottom line is, check with the SMPS vendor on whether it will work with a DC applied.
And if so, what the VDC should be.
Hi Ed,
Thanks for the detailed information.
My question is if it is universal standard input range it suppose to work from 85or90VAC, then for 85VDC the peak is 120VDC. Considering this 110VDC input may not create that much problem.
If my circuit employed with PFC booster then this 110VDC may be good enough to work because it provide steady voltage not like AC.
correct me if im wrong .