This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3406HV: Power ON

Part Number: LM3406HV
Other Parts Discussed in Thread: LM3406

Hello Team,

I use the LM3406HV for dimming a LED CHain of 12 High Power LEDs. The Input Voltage is DC48V.

When I connect the VIN Pin to the Power Supply, the LEDs lights at full power. After Power On Time the LEDs are OFF and the I can DIM the Brightness.

My Problem, the LEDs must be OFF at Start Up. When I turn ON the Application the LEDs must be out. When the Controller is working then the LEDs can be dimmed to maximum.

So how can I solve the Problem? Can anybody help me? 

Maybe is there an another Chip with VIN to 75V?