Other Parts Discussed in Thread: TPS73433-Q1, TPS7A53-Q1
Question on operating the LDO in an over current condition at startup. would like to use this TLV70012QDDCRQ1 LDO to feed a DC-DC boost converter which converts 3.3V to +5V. The boos converter has an inrush current requirement of 2.6A for 500uS however the DC-DC will boot in at lower input current levels. Since the LDO can not supply the 2.6A I expect that the LDO output will fold back and reduce the output voltage/current. The effect of this is to stretch the boot time of the DC-DC from a few mS to approx 50mS. The question is whether there is a reliability issue operating the LDO in this mode where it limits current for 50mS. Once the +5V supply boots the constant current draw is only 30mA.