I am using the TPS23754 in a fly-back topology.
The input voltage can be 24V via midspan or 48V PoE.
The output voltage is 5.5V 2.1A.
I started with a 10V auxiliary winding which appears just too low at 24V input and low loads.
Now I want to increase the auxiliary winding to 11V.
What is the recommended auxiliary winding voltage?
Regards,
Harold