Dear TI Experts,
I cannot find CCT bit in BQ27542, does this mean that Cycle Count Threshold only relevent to DesignCapacity()? Then if I set Cycle Count Threshold to 90% DesignCapacity, after 1~2 years, battery reduce to <90%.
Will Cycle Count stop to increment? If so, I suppose it should set Cycle Count Threshold to a lower value close to batery EOL reduction percentage to keep Cycle Count going.
Is the Cycle Count crucial to IT algorithm or just a reference to user to count the battery cycle and don't have influence to gauge?
Could you kindly help to give some advice about it?Thanks a lot.