The package limited abs max Id current is stated to be 200A in the datasheet for this device. This seems large considering the size of the leads for the TO-220 package. Is the 200A rating only good for a fraction of a second? If so, is there a way to approximate max continuous Id assuming very good heat sinking?
Respectfully,
Lucas