This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL7700: TL7700 Application

Part Number: TL7700
Other Parts Discussed in Thread: TPS3710

Dear Support,

I would like to use the TL7700 to monitor a 12V rail.  The RESET should trigger if the input voltage drops anything below 9V.  I am struggling to determine the resistor values required to set the trigger and hysteris.