Other Parts Discussed in Thread: GPCCHEM
Hello,
We are using the BQ27421-G1A for a Li-Ion battery pack (Tenergy 5200mAh 31001) and are experiencing serious issues with the TI part. The battery never reaches the terminate voltage of 3.2V, and I believe therefore is reporting inaccurate Qmax and SOH after just one charge cycle. This is a repeatable issue, and these are new battery packs.
I have a few questions:
- Is the part meant to work for a battery pack consisting of multiple cells in parallel? I assume so, but this is not explicitly called out in any documentation.
- Why would the gauge never reach the set terminate voltage of 3.2V?
- If the part is on a PCB and NOT located near the battery pack, would the temperature read by the part cause significant capacity errors?
- Why is the device accumulating error? Our SOH starts at 92%, then drops to about 83% after the first cycle, and then 75% for the third cycle, etc.
Can someone please help provide some insight into what could be causing out problem? Any help would be greatly appreciated.