The TPS62801 datasheet states an effective output capacitance of up to 26uF. Is this referring to the nominal value of the output cap or should I be derating the output cap for DC Bias and other similar effects first?
Also, what if I have other bulk caps (or other devices) in my design connected to this voltage? Do I need to include these when determining if I am less than 26uF or is it only the output cap(s) that are physically close to the power supply IC?
Regards,
Matt