This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53647: TPS53647

Guru 13485 points
Part Number: TPS53647

Need a very small design design solution for 12V to 0.9V/120A

The solution should be very small-current area is 37 x 45mm.

The c.s.height could be till 10mm

The p.s. height is 2.1mm

Is the TPS53467 is the best recommended solution for such design?Note: No need for PM BUS