Other Parts Discussed in Thread: BQ50002A
Hello,
I have a problem using the BQ51050B wireless charging receiver. I'm using it to charge a standart 500mAh Li-Ion battery.
Here is my schematic with all used values for caps and resistors (in brackets are the recommended values taken from the datasheet):
As I don't know the exact data from the receiver-coil I went for C1 and C2 in the recommended range stated in the datasheet for a "common" coil.
My used components are like the ones from this set (I removed the electronics from the receiver-coil and only used the coil itself)
In my first try I used 47nF capacitors as CCOMM. The CHG-Pin went low and high every second or two. My charger indicated connection to a receiving device while the pin was low and no connection when it was high. I then changed to 33nF caps for COMM with similar results (only the interval of low/high was longer). Then I changed the caps to 15nF and got it to work and charge the battery properly. The output voltage was ok and the current flowing to the battery was more or less as calculated and constant (CC phase of charging). But after 2 minutes (and no external interference) the mess started again and charging stopped. The CHG-Pin started toggling again. I still measured about 80mA flowing to the battery most of the time and sometimes little spikes of current. But the voltage on the battery was not higher than V(bat) without the charger, so there was no proper charging anymore. I restarted the transmitter-coil but wasn't able to reproduce the stable charging scenario anymore.
Playing around with different additional C1 and C2 capacitors there still was no improvement. Though after reverting back to the previous design without those additional caps it suddenly worked really good. So after all it seems that the design is not very reliable at the moment.
I'm not that much into Qi-charging, so I can't estimate the influence of different cap-values in the design and how much they effect it.
Where could my problems come from?
Regards
Daniel