Part Number: BQ27426
Other Parts Discussed in Thread: GPCCHEM
Hi
Please confirm about following question.
(Q1)
The document(slyt321) states that OCV will be measured when power is inserted.
Does this mean that OCV is measured after power is supplied to the IC?
In that case, the OCV can not be measured correctly because the voltage value is not in the no-load state?
(Q2)
The document(slyt321) stated that the value of Qmax will be updated by the second measurement of OCV.
Since the OCV is not measured unless the system enters the relax time, does the error of Qmax and SOC in the interval remain?
Or is the Qmax value updated during charging / discharging?
(Q3)
Does the IC have an OCV profile for each temperature?
Or is there an equation for calculating OCV that corrects the influence of temperature?
(Q4)
Does relax time mean the state where the voltage becomes constant with the load current I = 0?
In that case, since the current does not flow through the IC, the IC may not start up.
Or can it transition to relax time if the internal resistance is negligible micro current?
However, depending on the product, if the load current is always large, it is impossible to estimate the remaining amount because it can not transit to relax time?
Best regards,
Chiaki Endo