Dear Sir,
The transformer used in LM5041EVAL board is having 1.25mH primary inductance. (Np :8T, Ns: 1T)
in LM5041 the input is 35V-70V then after buck stage it'll be around 22V then current fed push-pull stage, which is having transformer which has a secondary of 2.5V.
1. From the core datasheet the AL value should be around 24000 nH/T2. is it correct?
2. This much big AL value core is required or around 5000nH/T2 is fine . magnetizing current will be high or which loss I have to consider in this scenario.
3. What will be the minimum primary inductance required for a current fed push pull stage transformer. (any reference document)
Thanks & regards,
Nesh