Part Number: LM5034
Hi,
We are using LM5034 to convert 48V to 5V (single output). I have pain full problem like some of the board will burnt (Switching FET) during testing because of high current flow in secondary winding of isolation transformer (Current Transformer) (4:1) and unfortunately we couldn't find the actual reason for it, but observed similarity in failed/burnt board that was solder balls presented in secondary winding of same transformer, my dilemma is whether this solder balls will cause huge current flow in secondary windings or not?
Thanks in Advance.