Other Parts Discussed in Thread: TPS3831, TPS3890
Hi team,
customer would like to use the reset IC as below requirement. Could you give me the datasheet and suggestion part with minimum package size?
Below is our application:
1. Vin abs. 6V and VIN min. <2.4V
2. Vout current capability is 10mA at least
3. Delay is needed when Vin from low to high, Vout delay for a specific period then output.
4. Delay minimum time is 60ms at least (fixed or programmable by external capacitance)
is TPS3831 ok for this application?
BR,
SHH