I am using LM2623MM boost converter in my circuit. As you can see from the datasheet when EN pin is pulled to ground, boost converter is disabled. I am thinking about supplying GPS and GSM module from this boost converter and I would like to cut off the power(for low power consumption) of them pulling EN to ground. My supply voltage of boost converter is 3.7V. As I researched when boost converter is disabled, output voltage becomes Vin-0.3V which makes 3.4V(not sure about that). Working voltage of GSM module is over 3.5V, GPS is over 3V. So does these components consume power, even if boost converter is disabled?