Other Parts Discussed in Thread: LM5117, CSD18504Q5A
Hi
Simulation of LM25117 on WEBENCH.
Input 4.5V~36V, output 3.65V/8A.
MOSFET M2 has a high temperature (Tj greater than 100 degrees C).
Is there a recommended MOS model to reduce the temperature?
In addition, LM25117 on WEBENCH
Set the input voltage to 4.5V~24V and output 3.65V/8A.
Why can't it be simulated?
Thank you.
Jerry