Other Parts Discussed in Thread: BQ24171
First, a development kit was purchased [BQ24170EVM-610-5V] which is used to charge a 3.7 V cell up to 2 A (maximum up to 4 A) of current. This kit has been modified to adapt it to a 12 V supply [from a car battery], thus limiting the charging current to the battery.
This same kit is intended to be used to be powered with a voltage range of 10 V to 14 V to charge 2-cell batteries [3.7V each, 2S1P] with a maximum recharger current of 1 A.
http://www.ti.com/tool/BQ24170EVM-610-5V
In the tests that were done, a laboratory voltage source with current limitation was used. In this way, it does not exceed the recharge current in the battery.
Identifiers/labels from components correspond at next link, page 18, schematic diagram.
http://www.ti.com/lit/ug/sluu463/sluu463.pdf
Voltage operating range: OPVSET
Supply voltage: + 12V
R_AC => R2 = 10 mOhms
Total current operating range: I_DPM
I_DPM = V_ACSET / (20 R2)
V_ACSET = 3.3 * (R18 / (R18 + R31))
R18 = 22k
R31 = 100k
V_ACSET = 0.59 V
R2 = 10 mOhms
I_DPM = 2.97 A
Current range of charge to the battery: I_charge
I_chrage = V_ISET / (20 R15)
V_ISET = 3.3 * (R30 / (R30 + R32))
R30 = 232k
R32 = 15k
V_ISET = 0.2 V
R15 = 10 mOhms
I_charge = 1.0020 A
R_SR => R15 = 20 mOhms
I_charge = 0.5010 A
Despite the changes made, the recharge current to the battery goes up to 4.7 A, The LED that indicates ~STAT is blinking when current is high but do not cut off supply to system neither to battery.
http://www.ti.com/lit/ds/symlink/bq24170.pdf
Changes of components made
R2: 0.01 Ohms
R6: 1 MOhm
R15: 0.02 Ohms
R18: 22 kOhms
R32: 15 kOhms
No changes in
R8, R9, R10, R19, R22
Should I use the BQ24171 integrated circuit?
Wish Parameters
Power Supply: +12 V
Current to system: 2 A
Current to recharge battery: 1 A [max]
Battery voltage: 7.4V [2S1P]
Kind regards.