This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90320: Figure 40 200ohms or 200Kohms? Which is correct?

Part Number: UCD90320

Hi,

In section 9.2.1 Design Requirements of the data sheet in Figure 40 it says to use a 200Kohm resistor.  However in the paragraph above it says to use a 200ohm resistor.   Which is correct resistor? 

Thanks,

HSG