Other Parts Discussed in Thread: BQ40Z50, BQ40Z50-R2
Dear Sir,
We are intending to use the BQ24773 in a portable electronic equipment for Battery Management.
Brief details of the Project is mentioned below:
1)Input to BQ24773: 18V to 22V
2)Type of Battery:3 Li-Ion battery pack
3)System VOltage: 12V to 14V
4)Max. System current: 2A
5)Max. Battery Charging current: 2A
The requirements/queries regarding this IC are
1)Does BQ24773 support Cell Balancing. If Not, kindly suggest any Texas Instruments Part
to be used along with BQ24773
2)How to monitor the current state of battery(percentage of charge left)
3)Is it necessary to monitor the battery temperature along with Voltage to ensure safety?
We look forward to you response,
Regards,
Sunil Kumar