This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25925: Response time for current limit function

Guru 19655 points
Part Number: TPS25925


Is there  response time spec for start current limit function on TPS259251?

Datasheet P6 is described t_FastOffDly at 300ns (and t_OFFdly: 0.4μs), but I look like P11: Figure 30 is more fast response (ns order) than P6.

I want to confirm correct response spec.

Or is OCP response time depend on condition? 

※Under reviewing current limit is 3.7A (R_ILIM: 100kΩ)

Best regards,

Satoshi