Other Parts Discussed in Thread: UCC256302, UCC28951
Hi,
do someone have used the UCC24624 duak channel synchronous rectifier in LLC topologie up to 3KW output power : 48V 45A.
The primary side is a UCC256302 controller.
My questions are about the beaviour of the UCC24624 in Burst mode with no load and restart after short circuit .
Do the UCC24624 is still used and tested with this power and under all these electrics stress?
Thank you per advance.