Part Number: LM3478
Hi
Is there a minimum load on the LM3478.?
When unloaded,the voltage shook.The cycle is 168 Hz.
The conditions are as follows.
input 13V~18V
Output 12V
SEPIC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM3478
Hi
Is there a minimum load on the LM3478.?
When unloaded,the voltage shook.The cycle is 168 Hz.
The conditions are as follows.
input 13V~18V
Output 12V
SEPIC