This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610: CycleCount() increment criteria

Part Number: BQ28Z610

Hello,

In the SLUUA65C is wriitten that the cycle count is incremented every time the discharge is greater than the value in CC_Threshold, whose default value is 90 %.

Different from other literature, in this one is not specified if the discharge is an "accumulate value"' or it is an absolute one. The difference is big, because in the latter case all partial discharges followed by charges won't be taken into account.

Then , if I read 299 cycles in the register, are they all continuous discharges from 100% to 10% or are they the sum of many partial discharge incremented every time their sum is greater than 90%?

Please, be so kind to give me an explanation as most exhaustive as possible.

Thanks a lot.