This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116: Need Schematic & PCB file verification .

Part Number: LM5116
Other Parts Discussed in Thread: LM25116, LM25145

Hello ,

One of my customer is working on Battery Charger project - LiFePO4 chemistry . 

In DC-DC section , i have promoted LM5116 device(in replacement for LTC device ) . this device will be scaled up & used in higher versions as well upto 18A requirement . 

Need help to verify the schematic & PCB files for the below input specifications :

1) I/P - 15.5V to 22V & O/P - 14.8V @ 4A

2) I/P - 25V to 40V & O/P - 29.6V @ 4A.

we can send the files for verification . please guide on how to move ahead on this . 

Regards

Mandar Mahajan

Arrow Electronics, India