Other Parts Discussed in Thread: UCC27714, UCC27712
Seniors:
I used the IR2110 driver to build a half-bridge arm drive circuit, as shown below:
The circuit is analogous to the recommended circuit of the manual.
The LIN and HIN pins have a PWM of amplitude 5V and duty cycle of 0.3. The 10V supply of VDD and VCC is stable, but LO and HO do not wave, LO is 0V, HO is 10V. .
Why is this?