Hello,
I am using LMR16006YDDCR based upon a WEBENCH design (thanks for that!). I have a question that will help in finalizing my design.
1. According to the datasheet, if SHDN is not to be utilized, installing a 100K resistor between VIN and SHDN is recommended. If one wishes to utilize the SHDN pin and do so from VIN, is it recommended that 100K be used as the value between VIN and SHDN and then calculate the value for the resistor between SHDN and GND accordingly?