This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61170: Efficient low-noise 48V Phantom Power From 9V Battery

Part Number: TPS61170

Hello,

the TPS61170 datasheet offers a circuit for 48V phantom power for condenser microphones. That circuit looks great but I'd like to make sure that it is the best solution for my purpose. Obviously, low noise is critical for these applications and I was wondering if TPS61170 is the best choice for that? My requirements are:

  • very low noise
  • high efficiency (long battery life desired)
  • less than $30 BOM
  • less than ~15 BOM count
  • footprint/height not relevant

I would be very interested in suggestions or experiences regarding other solutions than the TPS61170 phantom power circuit.

Thank you very much!

Sebastian