Other Parts Discussed in Thread: TPS723,
Hi Team
We find a question that LM2776 is work in PWM mode when the load current is 19 mA. But we can find LM2776 should be into PFM mode when the load current is below 40mA . What cause this ?
Another, When we move 3 pcs output capacitance closed LM2776 , and retain the next LDO TPS723 input capacitance. LM2776 work in PWM mode at any load. Do the circuit worl normal ?
PS: The value of C1+ between C1- is 104.